Default DDE Commands - These commands should be supported by your application.
+-------------------------------------------+---------------------------------------------+
| Server Command                            | Server Response                             |
+-------------------------------------------+---------------------------------------------+
| Server.Rev?                               | Return the revision of the DDE Server.      |
| Server.Terminate                          | Terminate the server if no clients are      |
|                                           | using it.                                   |
| Server.HostApp.Name?                      | Returns the host application name that the  |
|                                           | server form is running on.                  |
| Server.HostApp.Rev?                       | Returns the revision of the host app.       |
| Server.HostApp.Visible=(True/False)       | Shows or hides the server.                  |
| Server.HostApp.Visible?                   | Returns the current visiblility of the host |
|                                           | application.
+-------------------------------------------+---------------------------------------------+

AD9510 Evaluation Software DDE Commands
+-------------------------------------------+---------------------------------------------+
| Server Command                            | Server Response                             |
+-------------------------------------------+---------------------------------------------+
|                                           |                                             |
+-------------------------------------------+---------------------------------------------+